NR-V2X
|
SCPI Command |
[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:SLINk:BWP:ADD |
|
SCPI Example |
RADio:NV2X:WAVeform:CCAR0:SIDELINK:BWP:ADD |
|
Dependencies |
The maximum number of BWPs is 32. |
|
State Saved |
No |
|
SCPI Command |
[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:SLINk:BWP:COPY <integer> |
|
SCPI Example |
RADio:NV2X:WAVeform:CCAR0:SIDELINK:BWP:COPY 1 |
|
Couplings |
The maximum number of BWPs is 32. |
|
State Saved |
No |
|
SCPI Command |
[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:SLINk:BWP:DELete <integer> |
|
SCPI Example |
RADio:NV2X:WAVeform:CCAR0:SLINk:BWP:DELete 1 |
|
State Saved |
No |
|
Notes |
The minimum number of BWPs is 1. |
This setting is a read only setting.
|
SCPI Command |
[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:SLINk:BWP:COUNt? |
|
SCPI Example |
RADio:NV2X:WAVeform:CCAR0:SLINk:BWP:COUN? |
|
Couplings |
It is coupled with Add BWP and Delete BWP When Add BWP is executed successfully, this setting is increased 1 When Delete BWP is executed successfully, this setting is decreased 1 |
|
Preset |
1 |
|
State Saved |
No |
It is read only setting.
|
SCPI Command |
[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:SLINk:BWP<bwp>:ID? |
|
SCPI Example |
RADio:NV2X:WAVeform:CCAR0:SLINk:BWP0:ID? |
|
Preset |
0|1|2|3|4|5|6|7 |
|
State Saved |
Yes |
This setting is readonly and is the same with the carrier numerology.
|
SCPI Command |
[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:SLINk:BWP<bwp>:NUMerology? |
|
SCPI Example |
RADio:NV2X:WAVeform:CCAR0:SLINk:BWP1:NUM? |
|
Couplings |
This setting’s value will be coupled to be same with carrier numerology. |
|
Preset |
MU1 |
|
State Saved |
Yes |
Displays the BWP name with ID number appended to it. Read only.
This setting controls the RB offset of the BWP relative to CRB0..
|
SCPI Command |
[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:SLINk:BWP<bwp>:RB:OFFSet <integer> [:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:SLINk:BWP<bwp>:RB:OFFSet? [MAXimum|MINimum] |
|
SCPI Example |
RADio:NV2X:WAVeform:CCAR0:SLINk:BWP1:RB:OFFS 3 |
|
Couplings |
This setting is settable and readable. The maximum value of this setting couples with Max RB in the carrier. |
|
Preset |
0 |
|
State Saved |
Yes |
|
Min |
0 |
|
Max |
274 |
|
Resolution |
1 |
This setting controls the RB number of the BWP.
|
SCPI Command |
[:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:SLINk:BWP<bwp>:RB:NUMBer <integer> [:SOURce]:RADio:NV2X:WAVeform[:ARB]:CCARrier<carrier>:SLINk:BWP<bwp>:RB:NUMBer? [MAXimum|MINimum] |
|
SCPI Example |
RADio:NV2X:WAVeform:CCAR0:SLINk:BWP1:RB:NUMB 100 |
|
Couplings |
This setting is settable and readable. The range of this setting couples with RB Offset in current BWP and Max RB in the carrier. |
|
Preset |
273 |
|
State Saved |
Yes |
|
Min |
1 |
|
Max |
275 |
|
Resolution |
1 |